Hi all
My customer has built an inverting DC-DC with the TPS62160, 3.3V => -5.5V, similar to Figure 7 in the datasheet.
TPS62160 doesn't go below -2V. The IC heats up and consumes a lot of current but Vout is somehow stuck at -2V.
If Vout is set to -2V or higher (with R111,R113) the TPS62160 performs normal. VIN has been tested at 3.3V, 5.5V, 12V, no difference. In and out Capacitance has been increased without any impact.
At FB the Voltage -1.76V is measured. If Vout is set to -2V or higher the FB Voltage is -0.8V as described in the Datasheet.
Please find Figure 7 and the detailed customer schematic below.
Please review and comment.
Best regards
Ueli
---------------------------