This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53319: is there any method to convert -12V to -7V, -6A by a DC-DC converter or module?

Part Number: TPS53319
Other Parts Discussed in Thread: TPS5430, LMZM33604

in my system, there are only two input power rail: +12V,20A and -12V,-20A, (they come from an isolated DC-DC brick modules).

now I want to use a -7V, -6A voltage to supply the power amplifiers, can I convert it from -12V voltage? How?