Other Parts Discussed in Thread: OPA365, , TPS65133
Dear Madam, Sir,
I intend to use LM27762 in order to obtain +2.5 V and -2.5 V from a 5 V supply, to feed precision operational amplifiers such as the OPA365.
I downloaded the available SPICE model and am using it in a standard SPICE simulator. After importing it to the simulation tool, I built the schematic below:
While I do get the desired voltage level at the positive output, the negative output remains at 0 V. After running the simulation, I get the error message that the time step used in the transient simulation is to small. Is this a possible problem in the SPICE model? Is there another file I should add to the simulation tool besided the .LIB file?
EDIT: the Power Good PGOOD pin is grounded, simulation still results in 0 V at OUT_N.
Thank you.
Kind regards,
Luiz Guilherme Enger