Other Parts Discussed in Thread: BQ24296
Hello,
I'm not sure to understand the datasheet of bq24296M
In chapter 7.3 "Recommanded operation conditions" i read:
Isys - Output current (SYS) - 3.5A max
Ibat - Discharging current with internal Mosfet - 5.5A max.
Should i understand that my battery can deliver up to 5.5 A to system, when system is powered by the battery?
In this case what is the meaning of Isys, which is much lower?
Because the Mosfet (according to 8.2 Functional Block Diagram) is connected between SYS and BAT pins.
Thanks
Arnaud