Other Parts Discussed in Thread: BQ76952
Dear TI support,
My issue is very similar to this topic:
I would like to blow the fuse when CFETF or DFETF fail occours. I also would like to implement recharge protection when a cell voltage less then 2V on wake up from SHUTDOWN using CUDEP protection.
The settings below are not enough to blow the fuse on FET fail (DFETF, CFETF, PF_FETS, FETF_FUSE), also PF_FUSE should be set.
Since this point every enabled PF will drive the fuse.
So on the manufacturing line when BAT- and BAT+ connected/soldered/welded (should before connecting other cells VC1-VC9) the CUDEP is activated and fuse will be driven.
How I can prevent this?
Thanks in advance,
Attila