Hi TI Team,
I would like to ask if you could look over my design for the BQ24600, I have followed the datassheet and few examples as my guide when it comes to placing componenets and tracing, I'm just not houndred percent sure about the split of primary ground and analog ground. Please do give me your opinions and suggestions.
I've used the calculator that you have attached to the page of the device to scale compoenents to fit the specifications.
Specs:
- Cell Count : 6
- Vbat : 4.3 V
- Vbat : 25.8 V
- Ichg : 2 A
- NTC selected : ERT-J0EG103JAERT-J0EG103JA
Attached is PDF of the schematic and the top layer outline, as well as a PNG of both top and bottom layer.