Hi,
I have the same exact issue as in this thread here:
I have a 12V boost controller (MCP1665) connected to the output of the BQ25616 (SYS). I want to draw ~500mA from the 12V boost controller.
VBUS is 5.5V. D+,D1 are floating. I also tried to short D+ and D- to make the input current limit 2.4A.
With the battery connected (3.7V Li-Ion), I can draw the 500mA, but the battery is discharging even though I have 5.5V coming into VBUS.
I tried connecting VBUS directly to an external power supply just to make sure that it wasn't current limiting externally. I went all the way up to 13V and the battery was still discharging.
With no battery connected, the entire BQ25616 works fine until I try to draw any significant current (150mA on the 12V boost controller) - it then shuts down causing my entire board to reset.
The BQ25616 is completely powered up before I try to draw the current, so it's not the issue of the 200mA limit on startup.
Is the BQ25616 not designed to supply SYS directly from VBUS with no battery? It seems there are a lot of posts with this same issue with no solutions.
Here is my schematic:
Thanks.