Part Number: TPS51200
Dear TI specialists,
as some of the users have asked in this forum, we haven encountered during the design with the TPS51200 a problem with the overshoot on the REFOUT line.
Looking in the forums, we solved the issue by using a 4.7µF capacitor added to the line. As some smaller capacitors were already at the end of the line, we ended up with a capacitance of around 5.2µF.
As this solution solved the overshoot problem, it raised some concerns from our customer that increasing the capacitance might produce unexpected events that could affect the performance of the product, as in the datasheet is explicitly specified that the capacitance shall not exceed the 0.47µF. Therefore I have a few questions on these regards:
- What is the exact reason why this limit has been set?
- Will this limit be removed/adapted in the future versions of the datasheet?
- Is there any potential issue that might occur if a higher capacitance (>0.47µF and <10µF) is used?
Thank you very much in advance
Best Regards