This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
i have big problem with the IC ....
If the Battery is not connected and i connect the 26V input voltage,
the IC burns a hole nearby Pin 2.
I can reproduce this, this is not sporadic.
Sometimes i can burn the IC and the high Mosfet, if the Input voltage is 0 and connect the lipo.
Any Idea, waht is wrong?
Andreas
Hi Andreas,
What is the function and value of R22?
Regards,
Mike Emanuel
Hi Andreas,
Do you have an input blocking diode? If not, when you have the battery there is a path to short the battery to the 0 V input.
Regards,
Mike Emanuel