I copied the schematic in Figure 5 from the SLUSBN7D –JANUARY 2014–REVISED APRIL 2017 datasheet.
When I toggle the SW2 power switch on, I occasionally have no I2C communications. It does not acknowledge its address and the VDD pin 5 line is low. I've also seen large glitches, over a volt on the battery (pin 6 BAT) and I'm assuming they are related. Cycling power with SW2 clears it, but I need a robust long term fix. Short term should I remove some capacitors downstream of the SW2 switch in an attempt to minimize the power glitch? I really though the dual 18650 batteries would not dip in voltage.
I don't think it matters, but I did skip the one time programming step. I only need Voltage, Current, and Temperature data so I did not bother with the chip programing. At first I thought this was my issue, but I then saw the power glitch and VDD staying low.