Hi team,
I'd like to know if TPS61161A will work without problems in our conditions.
Based on the formula in the datasheet, it appears that 160 mA is the maximum output.
Since I plan to use 140mA output, is this a usable calculated value given the worst-case scenario?
*Conditions.
Vout : 25 V ( Typ 24V )
Vf : 0.6 V
Vin : 11.4 V ( Typ 12V )
Iout : 140mA
If not available, could you tell me about less expensive devices that can carry more current?
PWM control is a must.
Sincerely.
Kengo.