This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3817A: 400Hz operation 120W

Part Number: UCC3817A
Other Parts Discussed in Thread: UCC3817, UCC28064, UCC28180

Hi 

I would like to ask if this IC UCC3817 is capable of operating at 400Hz line frequency without any trouble and meeting DO-16 harmonics standard.

Do you have any application notes or proven prototype to support the application at 400Hz and 120W power AC-DC converter.

thanks in advance,

jun