This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
What is the main difference between BQ27220 and BQ27320?
These are both CEDV but I want to know how to decide which device to be selected.
Best Regards,
Yaita
Hello,
Both gauges are very similar. The BQ27220 has a greater Battery Capacity and it comes with pre-programmed chemistry profiles.
I have seen more customer use the BQ27220 due to its ultra power consumption in Normal mode and sleep mode. And this one has more documentation.
Regards,
Jose Couso
Hi Jose-san,
Thank you for your answer.
My customer considers to use BQ27220 or BQ27320 as a system-side gauge where the actual battery can be removed.
I believe he need to store learned gauge parameters like FCC and Qmax, etc in their system non-volatile memory before battery is removed.
On the other hand, BQ27520-G4 (Impedance Track Flash gauge) doesn't require the non-volatile memory.
Is my understanding correct?
Best Regards,
Yaita
Hello Yaita,
Correct, the BQ27520-G4 is a flash gauge. And so, it does not require to store parameters in host side in case of a removal of the battery. Cell information is stored in the device in non-volatile flash memory
Regards,
Jose Couso