This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: BQ25710 input current limit

Part Number: BQ25710
Other Parts Discussed in Thread: , BQSTUDIO, BQ25720

Hi

The customer use BQ25710. It can only drive 48W load. The input current is limited when it reaches 5.5A, and the IDPM is set to 6400mA in the software.

The same phenomenon with BQ25710EVM-017. The sense resistance is 10 milliohm. How to improve the input current capability

Waiting for your reply.

Thanks

Star

  • Hi Star,

    Can you send the register values when this is happening? 

    You can do this on BQStudio.



    What is the customer's input voltage, battery voltage, and ISYS load?

    Thanks,

    Peng

  • Hi Peng

    Thanks for your reply.

    Attached the schematic.

    * Created: Fri Feb 24 09:40:09 CST 2023
    *
    * Format: Register Name  tab Character,\t  Hexadecimal register value.
    * Device: bq25710
    * BQZ Container: Charger_1_00-bq25710.bqz
    *
    Charge Option 0	071F
    Charge Current Register	0BC0
    Charge Voltage Register	3328
    OTG Voltage Register	0000
    OTG Current Register	0000
    Input Voltage Register	0580
    Minimum System Voltage	2400
    Input Current Register	7F00
    Charge Status Register	8000
    Prochot Status Register	A800
    Input Current Limit In Use	7F00
    VBUS and PSYS Voltage Read Back	9100
    Charge and Discharge Current Read Back	0000
    Input Current and CMPIN Voltage Read Back	0000
    System and Battery Voltage Read Back	6301
    Manufacture ID Read Back	0040
    Device ID Read Back	0089
    Charge Option 1	0250
    Charge Option 2	021D
    Charge Option 3	0000
    Prochot Option 0	4A65
    Prochot Option 1	81A0
    ADC Option	A05F
    LOUT	0004

    1, Debugging found that the setting of Bit[4:3] (IL_AVG) of the register ChargeOption3 has an impact on the input current limit.

    I used to set it to 0-6A. Now after adjusting IL_AVG to 15A, the input current limit is normal. Will the setting of IL_AVG affect the current limit of the device?

    2, If I need a larger input current, the RSNS_RAC is set to 10 mΩ in the software, and the actual resistance is 5 mΩ. Is this method feasible?

    3, The input voltage is 12V and 19V, but our motherboard is designed to meet the power of 9-22V adapter, and the power of the motherboard is 100W when it is running at full power. The battery is 3 series, and the minimum voltage of the system is set to 9V, but the battery is not connected at the test stage.

    Waiting for your reply.

    Thanks

    Star

  • Hi Star,

    1. Yes. IL_AVG setting can affect charger operation because it affects the power stage. It is good to hear the problem is now resolved.

    2. BQ25710 only supports 10mohm current sense minimum. If they need 5mohm current sense, they will need to switch to BQ25720. Please see below comparison table



    3. I don't understand the question being asked or if they were merely stating their application, but it seems like the overall problem is resolved (by changing IL_AVG).

    Thanks,

    Peng