This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: Starting a high current battery charger design, is this the right part

Part Number: BQ24610
Other Parts Discussed in Thread: , BQ25730

Hello,

I am new to high current battery charger design but I have a design requirement where the circuit needs to charge a 4P12S battery pack. The design also has a "power path" requirement of being able to deliver 20A to the load source while also charging the battery. I think the BQ24610 could possibly work (though it says that is can support up to 6S batteries). My question is - Is there a better chip for this design and can I use the BQ24610EVM for initial evaluation