Hi TI Experts,
I have two questions about the resistance around the FB pin of the TPS54A20.
1. P32 of the TPS54A20 specification states "To reduce high-frequency noise, connect a resistor in series with the FB pin as shown in Figure 62", but what does it mean?
2. P24 of the TPS54A20 specification says "SLVA289 describes the reason for connecting the capacitor (C8) and resistor (R8) in parallel with the FB pin", but SLVA289 does not describe the reason for selecting the resistor, How were they selected?
Clippings of the relevant parts are included in the attachments. Please refer to