Part Number: BQ34110
Hi,
I have seen several threads where people have asked for customised coefficients for non-standard thermistors for the BQ34110. My enquiry is slightly different, I do not currently have hardware to test the thermistor, but I need to predict the temperature reported for specific resistances throughout the range of the thermistor. This is assuming using the recommended Semitec 103AT thermistor. I have tried modelling it using the conventional thermistor Beta equation but this gives errors at the low temperature end. Clearly the coefficients given in the reference manual indicate a different equation is used, presumably a polynomial. Apparently it is not the normal Steinhart-Hart type polynomial as the coefficients do not work in that. My question is - please can you tell me what the equation is that uses the coefficients so I can accurately model the temperature reporting?
Thank you
Regards
Chris Mayo