Other Parts Discussed in Thread: LMR36006-Q1, LMR36015, LMR36006, LMR36015S,
We measure LMR36015FSCQRNXTQ1 case temp at room temperature and would like to find out if running it at 80°C ambient would maintain junction temperature <150°C.
We follow two TI documents (LMR36006-Q1-thermal-case-study.PPT and Managing thermals with a 2-layer board deep dive).
We have the following questions:
- In the PPT: "PLOSS at 100°C ambient is calculated" --> this seems to imply that PLOSS is the same at 100°C as it is at room temperature - is that a safe assumption?
- The calculation in the PPT seems quite different from the one done in the deep dive". In the deep dive, how does one arrive at the 115°C max ambient in the last step (all previous steps are clear)?
- Also, the LMR36006-Q1-thermal-case-study.PPT doesn't seem to remove the inductor DCR losses.
- Bottom line, the two models appear to give us a significant difference in projected Junction temperature. Which of the two is right?
Also: Since the thermal shutdown will only kick in at 170°C, what will happen between 150°C (max Junction temp) and 170°C?
Thanks much in advance,
gj