This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65911: VDDCtrl current limit by RTRIP Resistor

Part Number: TPS65911

Hi support team,
Continuing from the "Original question" above.

Is the VDDCtrl current limit by RTRIP Resistor detected by the Low Side Valley current?

In that case, I think that "(IOUTmax - inductor-ripple-current/2)" is required for the calculation of equation (3), not "IOUTmax".
However, since there is no margin at all with this method, are you calculating with "IOUTmax" for convenience?

Regards,
Dice-K

  • Hi Dice-K,

    I believe the IOUTmax is related to the equation I found in this application note: Know Your Limits

    From page 8:

    In general, the valley current and the IOUTmax are similar since the second term in this equation is usually small but It looks like IOUTmax already takes into account the valley current.

    Regards,

    James

  • Hi James,
    Thank you for your reply.

    IVALLEY = IOUTmax - inductor-ripple-current/2
    The above equation is the same as the following equation (2).


    Since "inductor-ripple-current/2" is small,
    IOUTmax ≒ IVALLEY
    As such, does the equation (3) in the datasheet hold true?

    Best regards,
    Dice-K

  • Hi Dice-K,

    Yes, I believe this is why IOUTmax was used is equation (3) in the datasheet. You should be able to use that equation for the RTRIP calculation without significant error since the terms aren't too far apart.

    Regards,

    James