This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A11: Can the EN voltage exceed the IN and/or BIAS voltage?

Part Number: TPS7A11


Can the EN voltage exceed the IN and/or BIAS voltage?

Thank You,

  • Hey John, 

    This device can function with EN higher than VIN and VBIAS:

    As long as abs max is not violated:

    Please note when the EN pin is driven to a higher voltage than VIN, the current into the EN pin increases. If this increased flow causes problems in the application, sequence the EN pin after VIN is high, or to tie EN to VIN to prevent this flow increase from happening. If EN is driven to a higher voltage than VIN, limit the frequency on EN to below 10 kHz.

    Best,

    Juliette