Hi expert,
Customer used LM5050-2 to ORing DC_48 and BAT_48V. There is a question at DC_48V that when DC_48V was connected, then plug in BAT_48V and remove DC_48V, there is a short period of fluctuation during DC_48V decreasing around 36V. That seems DC_48V is charging and discharging. Is it possible caused by BAT_48V reverse current? Or do you have any idea what would it be?
Just to clarify, although we see the DC_48V fluctuation during transition at input, the ORing output for system can still normal operation.
Regards,
Allan