This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24624: UCC24624 : 86V Output condition?

Part Number: UCC24624
Other Parts Discussed in Thread: UCC24612, UCC24610

Hi,

My customer considers to use UCC24624 on LLC Converter for 86V output.  Is it no issue?  Please advise us. 

On this case (86V Output), my customer considers to supply Vdd pin from external 12V.  Is it no issues?   Please advise us.

Thanks and best regards,
M.HATTORI.

  • Hi Hattori-san,

    Yes, you can do this. You just have to clamp the maximum voltage that the VCC sees. Our application note SLUA860 shows how to do this with our UCC24610 and UCC24612 but the technique works with the UCC24624 as well. 

    I hope this answers your question.