This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 TS1 query

Part Number: BQ76952


Hi

The customer design with BQ76952, TS1 is configured as a 0x07 thermistor. Use the command 0x70 to get the temperature of TS1. When they disconnect TS1, the temperature value read is -60°C after conversion, This is correct. But when  they short-circuit TS1 , the temperature read is -31℃. 

It is normal if TS1 is not short-circuited. The disconnection value is about -60, but the short-circuit display is -31. The short-circuit should be a large value.

Does it normal?

Thanks

Star