Other Parts Discussed in Thread: TPS546D24S
Hello,
My customer is looking for a DC/DC converter for intel AgileX FPGA core power.
It is said that the core power of Intel Agilex FPGA is a PMBus Interface, which has limitations in that core power sequence and calibration must be performed normally.
The product previously used was VISHAY SiC450ED-T1-GE3 and was used under the conditions below.
- Input: 12V
- Output: 0.8V
- Max Current: 35A
- Supported PMBus Interface
Could you please recommend the optimal TI DC/DC conerter that satisfies the above conditions?
Thanks,
JH