Hello,
I disabled SLEEP mode with configuration Settings:Configuration:Power Config [SLEEP] = 0. Regarding completely disabling SHUTDOWN mode I went through FAQ (link).
Shortly - device goes in SHUTDOWN mode when:
- SHUTDOWN command is given
- RST_PIN is driven high for > 1 s :: I have connected this pin to GND permanently
- LOW BAT voltage threshold is triggered :: Up-on datasheet this threshold equals 4 V - 0.18 V = 3.82 V (max) or 3 V - 0.18 V = 2.82 V (min),
- Low stack voltage :: I'm using default value for threshold which equals 600 mV,
- Low minimum cell voltage :: I'm using default value for threshold which equals 0 mV,
- Over Temperature :: I'm using default value for threshold which equals 85 °C,
- Internal memory failure
How does the Internal memory failure looks like/how high is possibility that this problem arises?
I just to make sure that I can remove WAKE-UP switch permanently, since I really would like that IC doesn't go to SHUTDOWN mode, during battery is connected and electrical/temperature parameters stay within normal.
Many thanks,
Kind regards,
Dejan.