Other Parts Discussed in Thread: BQ40Z50
Hi
I have a query need your help.
If external balancing is used, the voltage sampling resistor of the first cell is 100 ohms and the voltage sampling resistor of the second cell is 5 ohms.
Do I need to replace it with a larger value? Like the BQ40Z50, if external balance is used, the sampling resistor should be changed from 100 ohms to 1kohms?
Please recommend the suitable resister value for external balance.
Waiting for your reply.
Thanks
Star