This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI experts,
My customer did EMI test with their own PCB using BQ25886.
They added C57 and R77 in the schematic below ;
and latest test result is as follows ;
Could you recommend the initial values of resistor and capacitor for this snubber circuit?
My customer wants get lower value of the range between 180MHz and 250MHz in vertical.
Best regards,
Chase
Hi Chase
The BQ25886 EVM has 10 ohm (R8) and 110pF (C13).
Also see application note on snubber circuits application in boost converters, SLVA255.
See E2E post on BQ25886 with a similar problem, BQ25886: FCC certification issue.