Other Parts Discussed in Thread: LM3444
Hello guys,
One of my customers is considering using TPS92074 for their next products.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
They want to add TPS92074 enable (LED on/off) function.
Do you know how to add the function?
Is it a way to add NMOS FET VSEN and GND?
I think LED is off (TPS92074 is disabled) when the NMOSFET is turned on and VSEN = L.
Q2.
They want to need a AC/DC LED driver which has the following function.
If you know any device which can achieve the functions except TPS92074, please let me know?
- Controller type (External switching FET type) (Mandatory)
- No isolated (Mandatory)
- Enable (LED on/off) control by digital signal (Mandatory or alternative way is mandatory)
- PFC type and No PFC type (They want to know one device at least for each type)
- Over voltage protection.
- Input voltage : AC100V +/- 15V before diode bridge.
- Output power wattage is about 12W.
- Output voltage max: 35V.
- Triac dimming is not needed.
Your reply would be much appreciated.
Best regards,
Kazuya.