This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The 1Kohm resistance was added between EN-GND for troubleshooting during the test.
And there was no problem when the ON/OFF test was conducted.
Is there anything that could be a problem by adding resistance?
If so, what additional tests should I try
Thanks
Hello David,
One problem might be the constant leakage current. Depending on the voltage at EN in 2-wire mode, with 1-kΩ pulldown at EN the leakage current can be anywhere from 6.5-mA to 48-mA. Increasing the external EN pulldown resistor to 100-kΩ can reduce the leakage current to 65-uA to 0.48-mA.
Best regards,
Tilden Chen
Solid State Relays | Applications Engineer