Hi
The customer design with BQ76930, the customer designed two versions of the circuit.
The first version was successful, but the second version had problems. The only difference between the two versions was the change of the power supply circuit to 12V.
Attached the schematic.
The registers all can be read, but the cell voltage is almost 0, and the temperature value is 0xFF.
Please give some suggestions.
Thanks
Star