This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: LM27761 output Voltage ripple

Part Number: LM27761

Hi Sir,

Could you support to provide output voltage ripple curve as following condition ?

1. Vin =3.6 ~ 5V ,Vout= -3.3V,Iout =5mA

2. Vin =3.6 ~ 5V ,Vout= -3.3V,Iout =100mA

2. Vin =3.6 V ,Vout= -3.3V,Iout =1/5/10/20/100/200mA

Simulation or test is OK to me.