Other Parts Discussed in Thread: SN65HVD235, TLV9154
Hello,
we intend to use the TPS560430X to convert 24V Vin to 5V. From these 5V we use an LDO TPS70933 for 3.3V.
We need the 5V for some OpAmps and the 3.3V only to power a small uC and a CAN-Tranceiver with around 30mA.
The Design for the TPS560430 was done with the help of WEBENCH.
We tested the design without any load. Therefor no other parts, exept those needed for the supply, were placed. In this case we achieved an output of 5.05V and 3.28V, which is good.
As soon as we added some loads, the 5V dropped to around 4V. The current remained at 5V remained low at a few 10mAmps. No devices ran hot.
I tried swaping the converter, increased the output capacitance, enlarged and lowered the inductance. All of that did not help.
Any idea why the TPS560430X is not regulating the output voltage to the desired 5V?
I added a screenshot of the schematics.
Not sure if it is needed, but on 3.3V there is the uC TMS320F3800137 and a CAN-Tranceiver SN65HVD235. On 5V there is only one TLV9154.
Thansk you for any answers.