Hello,
in reference to an ongoing issue, see here: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1285673/bq34z100-soc-jumps-rfrom-7-to-100-to-0
We changed the Firmware for this BQ34Z100-G1 to the Firmware recommended: 0.16, after some bugs occured with the FW2.01 for -R2.
We use ChemID 2100, as per the GPC_report attached. ChemID was issued under FW 2.01 on BQ34Z100-G1 (see old issue).
The datasheet of the used Battery is attached as well.
After changing to FW 0.16, Update Status won't change from 05 to 06. Logfiles, Logerrors and CSV of DataTables are attached as well.
Mon Feb 12 08:17:04 CET 2024 Time,LogCaption,Error Code,Error String 2024-02-12 08:17:04,Voltage,772,No acknowledge from device.2024-02-12 16:21:52,AverageTimeToEmpty,8,EV2X00 Adapter USB Timeout.2024-02-12 17:24:06,RemCap,772,No acknowledge from device.2024-02-12 17:43:18,CtrlStatus,8,EV2X00 Adapter USB Timeout.2024-02-12 17:56:19,RemCap,8,EV2X00 Adapter USB Timeout.2024-02-12 17:56:37,Current,772,No acknowledge from device.2024-02-13 03:34:12,Current,8,EV2X00 Adapter USB Timeout.2024-02-13 07:30:02,MaxError,8,EV2X00 Adapter USB Timeout.2024-02-13 14:20:12,Control,772,No acknowledge from device.2024-02-13 14:20:12,StateofCharge,772,No acknowledge from device.2024-02-13 14:20:12,MaxError,772,No acknowledge from device.2024-02-13 14:20:12,RemCap,772,No acknowledge from device.2024-02-13 14:20:12,FullChgCap,772,No acknowledge from device.2024-02-13 14:20:12,Voltage,772,No acknowledge from device.2024-02-13 14:20:12,AverageTimeToEmpty,772,No acknowledge from device.2024-02-13 14:20:12,AverageTimeToFull,772,No acknowledge from device.2024-02-13 14:20:12,AvailableEnergy,772,No acknowledge from device.2024-02-13 14:20:12,AveragePower,772,No acknowledge from device.2024-02-13 14:20:12,InternalTemperature,772,No acknowledge from device.2024-02-13 14:20:12,CycleCnt,772,No acknowledge from device.2024-02-13 14:20:12,StateofHealth,772,No acknowledge from device.2024-02-13 14:20:12,ChargeVoltage,772,No acknowledge from device.2024-02-13 14:20:12,ChargeCurrent,772,No acknowledge from device.2024-02-13 14:20:12,PackConfig,772,No acknowledge from device.2024-02-13 14:20:12,Flags,772,No acknowledge from device.2024-02-13 14:20:12,Flags B,772,No acknowledge from device.2024-02-13 14:20:12,GridNumber,772,No acknowledge from device.2024-02-13 14:20:12,LearnedStatus,772,No acknowledge from device.2024-02-13 14:20:12,DoDatEOC,772,No acknowledge from device.2024-02-13 14:20:12,Qstart,772,No acknowledge from device.2024-02-13 22:59:22,GridNumber,8,EV2X00 Adapter USB Timeout.
Chemistry ID selection tool, rev=2.54 Configuration used in present fit: ProcessingType = 2 NumCellSeries = 1 ElapsedTimeColumn=2 VoltageColumn = 9 CurrentColumn = 10 TemperatureColumn = 12 Best chemical ID : 2100 Best chemical ID max. deviation, % : 2.86 Summary of all IDs with max. DOD deviation below 3% Chem ID max DOD error, % Max R deviation, ratio 2100 2.86 0.33 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27421-G1D: 4.4V LiCoO2 18.93 354 bq27411-G1C: 4.35V LiCoO2 21.4 128 bq27421-G1A: 4.2V LiCoO2 35.62 312 bq27421-G1B: 4.3V LiCoO2 43.18 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 21.4 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 26.15 1202 bq27621: (default) 4.2V LiCoO2 27.15 Best generic ID 354 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 18.93 3230 bq27426: (default) 4.35V LiCoO2 21.34 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 27.15 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule