This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Questions about Qmax and RA update rules

Part Number: BQ27426

Hello,

Q1、What is the basis for the Qmax update rule 10°C - 40°C setting?

Q2、QMAX update rule 10°C - 40°C. What is the modifiable range?

Q3、QMAX update rule 10°C-40°C, don't quite understand your reply. Is there a specific example or a detailed formula for the effect on Qmax for temperatures above 40°C or below 10°C?

Q4、What is the DOD error that will limit the Qmax update?

#5: Because DOD=f(OCV, T). The gauge uses a cell model with characterized OCV normalized at one temperature and a mathematical model to calculate OCV(T). This model is an approximation of real cell behavior so if temperature is too high or too low, the potential DOD error becomes unacceptable for Qmax updates.

Q5、Based on your reply, our understanding is that in applications where the discharge current cannot be controlled, since there is no guarantee that it will always fit with 30 seconds, the discharge current has to exceed 123mA at all times during the discharge process. 
Is the understanding correct?

#2: The current must be above C/10 for each resistance measurement. If the current is below C/10, the gauge will not qualify a *specific* resistance measurement. The current can be below C/10 temporarily, may not affect Ra updates, if this is short enough for it to not coincide with a resistance measurement.

#3: The gauge takes resistance measurements every 30s once DOD conditions and transient time conditions allow.

Q6、The discharge current was basically around 100mA when we measured it, and there is no guarantee that the resistance measurement meets 123mA every 30 seconds. but the Ra Table was updated during the discharge, what is the reason for this?Is there any other factor other than the C/10 that can cause the RA to be updated?

Current data,pls check the attach-->sheet[Q7]。

Q7、The C/10 is not met but the RA table has been updated, is the Ra Table accurate at this point?

Q8、if our equipment has a maximum current of about 50mA during discharge, can it be modified to C/25?
What are the effects of this modification on the FuelgaugeIC's?

Current data,pls check the attach-->sheet[Q9]。

Q9、If there is reserve capacity, C=design capacity-reserve capacity, is this understanding correct? That is, reserve capacity 350mAh, design capacity 1230mAh, C/10=(1230-350)/10=88mA.

Q10、What is the basis for updating the rules for QMAX to be set to 37% of Qmax by charge? Please explain the following by formula or other information.

2043.Current_Data.zip

  • A1: The basis is in the method that the gauge uses to model OCV as a function of temperature.

    A2: 0deg.C and only limited by max signed int /10.

    A3: Qmax relies on DOD and DOD is a function of OCV measurement and temperature measurement. The gauge models OCV over temperature. This mathematical model isn't accurate enough for temperatures below 0deg.C and above 40deg.C to accurately determine DOD, hence the gauge excludes OCV measurements outside this temperature range.

    A4: The DOD error is the difference between true DOD and measured DOD.

    A5: For practical reasons, the discharge current should exceed C/10 during a discharge for the gauge to measure Ra.

    A6: No. Ra will not update if the current is less than C/10. This is a hard requirement.

    A7: The Ra table will not update if the current is less than C/10.

    A8: It can be modified to C/25. But the gauge's analog front end and integer math doesn't support Ra updates for C/25 so this is not supported by TI.

    A9: Reserve capacity is subtracted from capacity predictions. It is not subtracted from Design Capacity. Design Capacity is a reference capacity. The gauging results do not use Design Capacity in a simple formula but instead the gauge models a discharge scenario. It will then subtract Reserve Capacity from the results.

    A10: The basis is empirical data by the team that developed the algorithm. 37% DOD change was deemed the minimum acceptable limit for Qmax updates.

  • Hello dominik,

    1、The minimum value of Design Capacity in TRM is 0. If the Design Capacity of the battery is 500mAh, then C/10=50mA, can it make Ra update?
    What is the difference from (Design Capacity=1230mAh,C/25=49mA)?

    2、What is the minimum discharge current supported by the TI algorithm to bring the RA updated?

    A8: It can be modified to C/25. But the gauge's analog front end and integer math doesn't support Ra updates for C/25 so this is not supported by TI.

    3、Can it be amended to C/13 and what are the implications?

    4、Can it be amended to C/15 and what are the implications?

    5、Don't quite understand this statement, can you elaborate more?

    A9: Reserve capacity is subtracted from capacity predictions. It is not subtracted from Design Capacity. Design Capacity is a reference capacity. The gauging results do not use Design Capacity in a simple formula but instead the gauge models a discharge scenario. It will then subtract Reserve Capacity from the results.

    6、Can you provide information or screenshots of the conclusions of the 37% test data? Purpose: We may modify the parameter "Min % Passed Chg for Qm", so we would like to know the steps and criteria to determine the accuracy of Qmax.

    A10: The basis is empirical data by the team that developed the algorithm. 37% DOD change was deemed the minimum acceptable limit for Qmax updates.
  • #1: Yes, if the current is above C/10, then Ra can update. It's not just about the absolute current 50mA vs. 49mA in your example. Besides having a reasonable current (the gauge uses a 1mA resolution and integer math so this limits accuracy if absolute currents are small), there also has to be a significant voltage drop OCV vs. loaded voltage and that is what makes a difference between your 500mAh and 1230mAh example. 50mA for the 500mAh cell will produce a larger voltage drop than 50mA for the 1230mAh cell (the latter will not produce enough voltage drop, hence the gauge can't measure Ra).

    #2: It's C/10. There is no absolute limit. The Ra calculation will become less accurate for lower absolute currents. You can calculate an error for a specific case using integer math (e.g. if your true current is 1.5mA but the gauge measures 2mA (because of the resolution) and your true voltage drop is 10mV but the gauge measures 9mV, then you can calculate the error as Rmeasured = 9mV / 2mA = 4500mOhm with Rtrue = 10mV / 1.5mA = 6667mOhm).

    #3 and 4: Yes, it can. See answer #2 how this will impact the Ra calculations.

    #5: Remaining Capacity = Simulation Result - Reserve Capacity.

    #6: No.

  • hello Dominik

    The discharge current of our application does not satisfy the C/10 rule. So we need to modify the rule of discharge current C/10.

    1. What does 'C' in C/10 stand for? What is the value corresponding to 'C' in our configuration?

    2、Modify C/10 to C/13, how much error will RA have?

    3、Modify C/10 to C/13, how much error in RA will lead to error in FCC?

    4、Modify C/10 to C/15, how much error will RA have?

    5、Modify C/10 to C/15, how much error in RA will lead to error in FCC?

    6. To modify C/10, should modify the FS file? Can you help to provide the two FS files for C/13 and C/15?

  • #1: C stands for C rate in [h]. It's a way to specify load as a function of Capacity. C/10 equals a current of DesignCapacity / 10[h] (a current that would accumulate to Design Capacity in 10 hours).

    #3-5: This depends on the chemistry and can't be determined with a simple formula. It would have to be analyzed separately for a specific cell and chemistry.

    You are trying to "fix" the algorithm's configuration in a way that will break it, not make it work. These parameters are private for this reason. The gauge won't be able to measure Ra reliably for smaller currents than C/10.

  • Hello Dominik,

    Since our equipment has a minimum discharge current of 100mA, please help us with the corresponding FS file for C/13. Thanks!

    We need to do the verification to confirm if we can modify the parameter.

  • A configuration file with min. res current C/13 is attached: https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/0426_5F00_2_5F00_02_2D00_bq27426G1_5F00_C13.gm.fs