This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2813-0: VCC Current way above limit for safe operation

Part Number: UCC2813-0

Flyback Circuit - 02.21.24.pdf

I am having problems with what I think is overcurrent on the the IC that causes it to break down after some amount of time. I have broken the trace on my board and added a wire to measure the current on the VCC pin of the IC. I am also measuring the voltage at the CS pin with an oscilloscope. 

These are the values I am seeing with the attached schematic: 

I_VCC:

  • Max = 168mA
  • RMS = 16.68mA

V_CS:

  • Max = 1.68V
  • RMS = 332mV

Based on the datasheet, the current at VCC is WAY too high (it should be <30mA) and the voltage at CS is higher than 1V. What can I do to decrease this current and voltage to ensure safe operation with this IC?