Other Parts Discussed in Thread: TPS61023
Hello,
I am planning to use the IC TLV61070A in boost mode for my new design.
Below is the requirement,
- Input voltage : 1.5VDC to 3.2VDC
- Output Voltage : 5VDC
- Outlut current : 500mA to 750mA
Kindly review the requirement and suggest whether I can use the IC TLV61070A for this application?
I have seen that there is Encrypted PSpice Model is available for TLV61060A, Can I use that model to simulate the design?
Also you can suggest other boost IC which can meet the requirement.
Regards,
Alpesh