Other Parts Discussed in Thread: LM5121, LM5171
Hello,
I came across a similar question on the thread regarding the LM5122 current detection position (Previous answer from TI Forums). As was already answered, using CSP, CSN pins on the low side of the HB is possible but not recommended due to negative spikes during switching.
We are looking for a Synchronous Boost Controller like this LM5122 or the LM5121/-Q1 but we are managing a slightly higher input voltage. In the Datasheet it says that the recommended Vin, CSP, CSN voltages are 65V and the AMR are 75V. Our system is powered up by a Li-ion pack batteries in a 16s2p configuration, so the worst case could be when this pack is fully charged (16 cells x 4.25V = 68V) and the converter is "off" without load.
Would this situation cause any damage or excessive stress on the IC? Should we explore alternative components, or would the LM5122 be suitable for our application?
P.S. This battery voltage will drop immediately as the converter starts regulating the output voltage under load. Therefore, this worst-case scenario only occurs during brief periods when the converter is off or just starting up and the battery is fully charged.