Other Parts Discussed in Thread: LM2776
The datasheet says I can sim LM27761
webench.ti.com/.../quickview.jsp
The tool says part unsupported. Looking for +5 to -5 - Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I cam up with a 316K over 100K to get my -5V. (just used -1.22V and worked backwards.
I have the EVM and will test when resistors arrive. - Patrick
Hi Patrick,
FYI - The absolute value of the output voltage will be slightly lesser than the input because of the charge pump output impedance plus LDO dropout voltage. Please refer to Figure 19 and 12 in LM27761 datasheet.
If you want to just invert the input, you can choose the LM2776. It doesn't have the integrated LDO. So you wouldn't have the dropout across the LDO. Only the charge pump output impedance needs to be considered.
Best regards,
Varun