This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Power management forum

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: BQ34Z100-G1

Tool/software:

 I am looking at a 200 Amp peak and 100 Amp nominal discharge from my battery pack. And I need to use BQ34Z100-R2 which has Battery capacity (max) (MAh) 7000000 but the max input voltage is 125mV at SRN and SRP. I need to ask following two questions.

1) what should be the value of sense resistor in this case it should be   0.625mili Ohm (R=V/I is 125mV/200A) but in the previous post you recommended it should be minimum 2mili ohm for better performance. 

2) If the Battery capacity (max) (MAh) 7000000  for BQ34Z100-R2 then how it is being reflected in the hardware design.

 Thanks

Khalid Mahmood