This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543C20A: Switcher design assistance using TI calculator tool

Part Number: TPS543C20A


Tool/software:

Hello,

I am working on designing a power supply with the TPS543C20A. 

I will be using the TPS543C20A to step 14V Vin down to 1.35V Vout @ 25.5A Max Iout.

I don't have very many hard design parameters outside of that. I'd like a small enough ripple so that I don't see any switching artifacts on the output of the LDOs that the TPS543C20A will be providing the 1.35V to. These LDOS will be regulating the 1.35V to 1.2V.

As you can see by my provided information, I am by no means a power expert.

I've been working with the provided design calculator for the TPS543C20A. 

The first thing I've noticed is when I type in all of my parameters, the COUT values generated trigger a design caution:   

  

It looks like the tool is warning about too much output capacitance causing loop instability.

I began with the provided value but the undershoot and overshoot vout cells went red. There doesn't seem to be a value that will turn the COUT cell green. 

I was wondering if the TI team could sort of guide me through properly using the calculator as I don't have much(if any) design intuition on what the different values in the tool should be and am lacking most of the stricter requirement information that the tool allows you to design for and I would like to make sure I'm using sensible values at the least.

Any help that TI Engineers could provide would be greatly appreciated.

Thank you,

Matt

  • Hi Matt,

    Happy to help guide you through this design! As a starting point, would you be able to share your excel file here? I will make some tweaks to that, with a focus on low output ripple, and offer detailed explanations for each of the selections

    Best regards,

    Britton

  • Hi Britton,

    Of course. Note I didn't actually calculate a COUT value so the 1500uF there at the moment was just a value I entered when I was messing around with the tool. 

    Thank you so much for your help. Here is the file:

    3683.TPS543B20_TPS543C20A_TPS543C20_Calculator.xlsx

  • Hi Matt, 

    Attached below is the updated excel file with my recommended component selections. I'll explain the design choices that were made as well:

    1. Switching Frequency - Your selection of 1400kHz is a reasonable selection. This "high" switching frequency will allow you to achieve ripple requirements with a lower inductance and less output capacitance, which will ultimately reduce BOM costs. We categorize 500kHz as a middle ground frequency that balances solution size and efficiency, if you do not have strict efficiency requirements then I recommend the1400kHz selection for the above reasons.

    2. MODE - Enabling the API/BB with a mode resistor is by no means a requirement, but it does offer marginal improvements during a load transient. We typically enable API/BB when load transient requirements are strict. In your case, you can enable the API/BB feature or ignore it by leaving the pin open, either solution is perfectly fine. 

    3. Inductor - I noticed that you had a 1uH inductor filled in originally, I believe this was a source of some the issues/design warnings that you were seeing. I adjusted the inductor value to 0.1uH to match the target recommended inductor value for this application, which is designed to achieve a recommended 30% inductor ripple. The selection of 1uH is not possible for this application because the inductor ripple would be so low that the device can not properly sense current. I recommend the 0.1uH selection, but anything from 50nH - 200nH is acceptable. 

    4. Output Capacitors - I went ahead adjusted the output capacitor selection to reduce ripple as low as possible while maintaining stability. In this case, I chose 2x 330uF Bulk Capacitors + 6x 100uF ceramic capacitors. The 330uF bulk capacitors are not a hard requirement, but they allow us to achieve higher capacitance with a lower solution size. Ultimately, you are in the green if you have less than ~1300uF. There is a design caution on the feed forward capacitor, this is not cause for alarm and we always recommend to have a placeholder for the feed forward capacitor & resistor in parallel with the top resistor in the feedback divider. 

    When you design your schematic and layout, feel free to share them with me and I can double check the design before the boards are built! There are schematic and layout guidelines that you can find on a separate tab in the attached excel tool.

    3683.TPS543B20_TPS543C20A_TPS543C20_Calculator_TI.xlsx

    Best regards!

    Britton

  • Hi Britton,

    Thank you so much for walking me through this design.

    I apologize I forgot to supply you with all of the information. We actually do have an efficiency requirement, loosely it stated as " the higher the better". 

    It looks like ~ > 90% should be achievable with this part.

    Is there an indication in the excel design tool of what efficiency to expect with the current design?

    Will it be necessary to move up to 500Khz to reach the efficiency we are looking for?

    Thanks again for all your help,

    Matt

  • Hi Matt,

    The excel tool does not estimate efficiency but I can use our bench data (published in the datasheet) to make an estimation. To achieve a 90% ripple, I would recommend the 500kHz. With a frequency greater than 1MHz it will be difficult to achieve 90% efficiency at 25A load.

    Attached is an updated excel tool with 500kHz selected. The notable changes are the RT resistor to select frequency, the ILIM resistor to select current limit, and an increased inductor value. 

    3683.TPS543B20_TPS543C20A_TPS543C20_Calculator_TI (1).xlsx

    Best regards,

    Britton

  • Awesome. Thank you Britton.

    Once I've finished the circuit/layout I'd like to send it to you for a quick review if you don't mind. Should I leave this ticket open until then so I can upload it on this form?

  • Hey Matt, 

    Absolutely. I recommend creating a new thread when you complete the schematic & attaching the excel tool or a link to this thread in that new post.

    Best thing for our metric is to close tickets in a timely manner with the "Resolved" button. If you found the thread helpful, it is much appreciated if you can select the "Resolved" button 

    I look forward to reviewing the design

    Best regards,

    Britton

  • Hi Britton,

    Sounds good. One more thing.

    The chosen current limit value seems nonsensical, Should I just use the recommended value? Basically 30 A limit is great for us , so should a standard resistor value near the recommended here be chosen: Thank you

  • Yes that is correct. Any standard resistor value near the recommended value is okay

  • Awesome, thank you. I'm actually going to limit the current at 35A to start until we've tested our system a little more and have quantified load currents better. Resolving this thread. Thanks Britton. 

  • Hi Britton,

    Does this inductor look like a reasonable choice? 

    I basically picked it to have a decade higher SRF, and 2x sat and max current ratings, then .320uH inductance.

  • Hi Matt,

    This choice looks reasonable. The saturation current does not have to be 2x per say but should be above the desired current limit

    Best regards,
    Britton

  • Hi Britton,

    Looking back through the thread I realized we had discussed lower 100nH for the inductor. Could you explain the choice a little bit based on what's on the table here.

    Thank you,

    Matt

  • Hi Matt,

    The 100nH inductor was actually the recommended inductor for 1.4MHz frequency. When we adjusted the frequency to 500kHz, the inductor was adjusted to match. In the case of 500kHz, I recommend the 0.32uH inductor. 

    Best regards,

    Britton