This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
My customer are using Panasonic 18650 battery,Vin(max) = 9V, Vin (Min) = 5V
When Vin = 9V, it need charge the battery with 4.2V/2A charging current. and also provide 3.3V ~ 4.2V 1.8A to the system
When Vin = 5V , no need charging the battery, but need provide 3.3V ~ 4.2V 1.8A to the system
Can you help recommend a suitable device ?
thansk!
Hello,
Check out BQ25638.
Regards,
Mike Emanuel