This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We are using a BQ28Z620 BMS with LiPo batteries in 2s configuration and are having some issues having a valid SOC value.
When searching for the procedure to execute a battery learning cycle, we had trouble finding all the information, but we were able to find pieces of procedures in multiple documents and forum.
Here is the latest procedure we executed on a brand new BMS evaluation kit (BQ28Z620EVM-071).
After that, the SOC was tested by charging the battery to 100% capacity and discharching at a steady rate of 430mA (~C/5). The SOC, voltage and current was manually logged to observe the discharge.
We would expect the SOC to be mostly linear with a discharge rate that should match with the orange line for 2100mAh. However, the relative SOC procides invalid value and indicates 0% charge about 45 minutes before the real empty state.
Our application requires to have a good estimate of when the battery will be depleted, so we need to address this issue.
I also attached the golden image output files in case it can provide you more information.
20250123-BQ28Z620-LiPol Golden Rev2.0.zip
Thank you,
Sebastien
Hi Jonny,
Here is the report from the GPCCHEM tool and the measurement that was done to generate the file.
Note, I had to re-generate the report using the tool and the chemID changed to 1304 in the report.
Both 1210 and 1304 are LiCoCO2/carbon 11 type.
20250123-LiPol-Rev1-report.zip
I checked the document in the link that you provided (https://www.ti.com/lit/pdf/slua684).
I'm happy to see that the procedure in section 2.2 is the one I did with a constant current load and that my analysis is valid.
Let me know if you need other information.
Regards,
Sebastien
Hello,
I programmed your .srec file onto my EVM, and it appears that you have not successfully completed the learning cycle, and update status is still 0x04. Please ensure that you have successfully completed the learning cycle before referring to the SoC accuracy. You can refer to this application note on Successfully Completing the Learning Cycle.
Regards,
Jonny.
Hello,
Thanks for the tip. We are re-running the learning cycle as we speak. I should be able to validate if it solved the issue by the end of the week.
I'll keep you posted.
Thanks,
Sebastien
Sounds good,
Please update this thread if you have any other questions.
Regards,
Jonny.
Hi Jonny,
We have completed the learning cycle all over again. Everything went as expected, except for the update status register which is still 0x04 after the last relaxation. According to the procedure, the update status should change to 0x06 when the VOK bit is cleared. However, it did not happen.The log and golden image are attached with this message.
20250205-BQ28Z620-LiPol Rev2.1.zip
We have been trying to run the learning cycle (which takes multiple days each time) for a while now and it still isn't working. Do you have any idea why the learning cycle is not completing or if we can force the learning cycle to finish?
Thanks,
Sebastien
Hi Jonny,
I checked the post you provided. Looking at the log file, the DOD0_x registers were close to 90% change, but did not reach it most probably due to the batteries' internal protections when discharging. The undervoltage protection kicks in at 2.75V.
In the previous cycles, our charging voltage was set to 8.3V. Would increasing the charging voltage to say 8.4V or 8.5V help to increase the DOD0_x change?
Regards,
Sebastien
Hello,
I believe this would help, although I recommend making sure that you do not exceed the maximum spec of the cells.
Regards,
Jonny.
Hi Jonny,
Good news!
We successfully completed the learning cycle by increasing a little bit the charging voltage.
The Update Status went from 04 to 05 after charge and to 06 after discharge.
For anyone curious, here are the 3 things we did differently this time.
We did run the same kind of test as before to measure the accuracy of the SOC and the results are much better.
Thanks for your support,
Sebastien