Hi,
Customer of mine is evaluating TPS54394 for mini compo product. Per my understanding, TPS54394 has fixed switching frequency of 700kHz. This would cause TPS54394 to interfere with AM frequency. Attached please find the AM beat measurement being carried out by customer. The requirement is not to exceed 68dB.
Vin = 13V
Vout1 = 5.2V; Iout1 = 2A
Vout2 = 3.3V; Iout2 = 1A
Could you advise the following:
- Is there any way to adjust the switching frequency lower than 700KHz to avoid interference with AM frequency?
- if it’s not possible to adjust the switching frequency, is there any other counter measure to improve the noise?
- In datasheet (pg1), I noticed that the GND and PGND pin being grounded differently. However in EVM, both pins are grounded at the same plane. Could you advise which I should follow?
Thanks in advance!