This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello~
I have some questions for bq34z651.
1. SBS COMMAND 0x10 - Full Charge Capacity, To update this value (Full Charge Capacity), what value does bq34z651 refer??
To change this value (Full Charge Capacity), do I need to change the register value of any part??
2. SBS COMMNAD 0x0F - Remaining Capacity, This value is always not set above the "Full Charge Capacity".
Is it corrent??
Thanks... C.W. :)
C.W.,
The device will run simulations and update FCC and RM automatically and these are read only registers. RM should be less than or equal to FCC. FCC is the capacity available in a full pack and RM is the amount of capacity left in the pack.
Regards
Tom