This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
is there any one can help us on following
we need to change input voltage on following design from (36 to 75 volt ) to ( 18 to 36 volt ) , please let me know which element must be change in this design
thanks
david
Hi David,
If you change the input voltage, you need modify the the power components such as Primary Mosfet, transformer.
For the control circuit, follow the instructions in LM5025A spec to modify the components.
hi
many thanks for your reply , we solved our problem but i have another question
in this circuit +SB is trim pin and J8 is trim up and J6 is trim down or not ?
thanks
david
Hi Williams,
SB is secondary Bias.
J8 and J6 are sense pin which are used to compensate voltage drops on the output by sensing the actual output voltage at the load.
Regards