This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Forum,
I am searching for a switching IC that I can provide 15A preferred or at least 8-10A with a voltage range upto 50V or close.
I tried to search for one in the product list but couldn't spot one that had all characteristics. probably I missed.
Is there anyone who can provide me with a suggestion?
I want to alter its design to make a constant current supply. its described below. the IC mentioned cannot souse such high current. Im afraid if this IC is not available, I would have to bottom up design the whole circuit and if would take so much time I cannot afford to lose.
Any help would be so much appreciated.
This project is completed as a social service project. This circuit aims to provide power to a chemical extractor that extracts a certain chemical dissolved in the water in that area. project has hope it will help people a lot.
Hi Amalinda,
We don't have any Simple Switcher IC's that can directly accomplish this. Which is why Webench is throwing an exception.
I will repost this int the Non-isolated DC-DC forum to see if someone can help.
We are also working on a design that might achieve this, but the earliest I can get this out to you would be end of the week.
Thanks,
Anston
For a buck converter you will have to have an input voltage higher than the output voltage. For 750 W, you are definitely looking at a controller and likely an isolated solution as well or possibly multi-phase.
Dear Anston,
In that case i'm feeling lucky! :) you know I was thinking, may be I can combine the outputs of two or more switched mode ICs to achieve this current? But I understand that outputs cannot be directly connected at the end. So there must be some sort of a method to stop them from sinking/sourcing to keep them from killing each other. What do you think of my previous idea?
If you already know, could you please tell me a switched mode regulator IC that can pass at least 2-3A with approximately 50V output? If I can have that, then I can continue testing my idea on my initial diagram.
Well I am glad you are working on something similar. If you have any progress, please let me know and that would be so much helpful.
Dear John,
yeah, I am well aware of that. i think that will be my next biggest hurdle. Creating a power suply that can source such current at such a voltage. But I was thinking may be I should finish off the controller circuit first, test it and then move into to this.
Are your input and outputs finalized? If you still need 45-50 V input and 50 V output you are looking at an isolated solution. Let me know.