I have used the LMR12015 in two designs, one with and output at 3.6V rated for 500mA and one at 7.6V rated for 500mA load.
I have had no issues with the 3.6V design, this works well.
The 7.6V option is not good. There is a high failure rate of the device (>40%) when the supply is switched on and off a number of times.The failure mode is an increase in the current draw from the supply, it ranges from 50mA to a full short of the input.
I have attached details of the 7.6V circuit. LMR12015 circuit details for TI.docx
I have tested this circuit with a number of modifications, the first been an increase in the switch on load to 20mA. It is not clear in the data sheet how to relate the minimum startup current to Vout and L value.This did not make any difference.
I tried increasing the inductance value to 4.7uH. This has helped but the failure rate is still around 20%.
Below is the switching node and Boost node waveform for a working 7.6V output option with a 4.7uH inductor and 20mA startup load. In the same document is the switch node waveform were the current draw from the 12V supply has gone from 100mA to 135mA during a power up cycle.
LMR12015 waveform details for TI.docx
Is the oscillation after the NFET switching OFF correct?
How critical is the limit of the Switch Node minimum of -0.5V? On both the 3.6V and 7.6V options the Switch Node is dropping to below -1V for the soft-start period.
What is the effect of the oscillation on the switch node going above the Vsw level when NFET is ON?
Any help in trying to solve this would be great.
Many thanks
Luke