This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are two issues that makes me to ask for help:
First, In schematics of evaluation board and application notes related to LM5045, I couldn't find any type of snubber circuit on switches to reduce spikes.
does it mean that there is no needs of snubber for these circuits? If not required, how to reduce spikes on transformer windings?
The second issue is Powermos protection. In application notes Mosfets are connected directly to the driver pins from LM5045.
I did the same, but switches burned easily. Is there any need for mosfet protection?
I tried to add protection by placing 10ohm resistor in series with gate of each one.
Also since the absolute rating of LO1/LO2 , HO1/HO2 to HS1/HS2 are near vdd, and LM5045 would be damaged by spikes
I placed zener diode(12v) between gate and source of each mosfet which helped to elliminate this kind of LM5045 damage.
but the waveform of primary side winding of transformer altered and become asymmetric.
I would be appreciate any helps about snubber and protection.