Other Parts Discussed in Thread: UCC21520, UCC28C41-Q1, UCC28C43, TIDA-00199
I'm working on an open source 3-phase AC motor controller and came across a rather elegant 4 output isolated supply for the IGBT drivers. However the design is found in the LT3748 spec sheet, which appears to have limited availability. I would rather use a TI part such as the UCC28700-Q1. So my question is if this same circuit can be accomplished with this TI part or another TI Flyback controller.
The example circuit uses a 6 tap 1:1 VERSA-PAC VP4-0075-R transformer. 3 outputs for the 3 phase top IGBTs and 1 common output for all 3 bottom IGBTs.
I've attached a schematic of my current circuit design using the LT3748. I changed the MOSFET to be a FDD770N15A. I also made each of the secondary outputs split rail supplies using a 15V Zener diodes to create a 15V and -8V dual voltage supply. These supplies are fed as inputs to three UCC21520 half bridge IGBT drivers. The source voltage will be a 12V automotive supply and each of the top IGBT supplies should be at least 100mA and the bottom shared supply should be at least 300mA. Depending on the IGBTs I may need even more power, since they may be switching up to 600A of current, depending on the application.
The 6 tap transformer has an extra tap in this case which can be used as the aux winding. I would appreciate any and all feedback on the feasibility of using the UCC28700-Q1 for this application.
Best regards,
Element Green