This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
refer the LM2576 schematic above, it generates perfect 12V DC. But the output is observed to overshoot (>24V DC) when its output is connected as input to another synchronous regulator from Maxim-integrated as depicted below.
Objective is to augment an existing system that has +28VDC for generating five different tune-able negative voltage range -2.5V to -5V DC. LM2576 would step-down 28 to 12V DC and Max17502 in turn would convert 12V into -7V DC. Five LM337 parts would provide tune-able -2.5V to -5V DC from this -7VDC.
The second schematic works perfectly with 12VDC from external SMPS, but when cascaded to LM2576 setup above, causesLM2576 output to overshoot beyond +24VDC instead of stable 12VDC.
Please advice reason and possible solution such that LM2576 output is not impacted by input to Max17502H
I think John is on the right track.
I suggest two things:
Increase the SS cap on the MAXIM inverting Buck-Boost by a factor of 10 from 0.01 up to 0.1uF. This will slow down the ramp-up time of -7Vout.
Make sure the voltage divider on R2/R4 on the UVLO input of the MAXIM device is set for 10.5 or 11V so the first converter is nearly stable before the second converter attempts to start.